Leave a message
Custom and volume optical manufacturing with the expertise to guide you:
Knowledge Center/ Glossary/ Reference Wavelength
A wavelength, for example 632.8nm, for measuring the accuracy of an optical flat. A 1/20λ flat will have a maximum peak to valley deviation of 632.8/20 or 31.64nm. One wave is 632.8nm.
See also Surface Accuracy , Optical Flat