The polarizing film XP42 contains an iodine dye to obtain its light polarizing function. If the temperature of the film exceeds 80°C the polarizing component will be damaged. For applications up to approx. 100°C we recommend the polarizing film type XP40HT as this contains a modified polarizing component with improved heat resistance.